USB Portable License Overview
A USB portable license is locked to a USB dongle. When attached, the USB dongle provides a Host ID, which unlocks the license file is that installed on the hard drive. USB portable licenses require the installation of a Dongle Driver package. See the Keysight Software Manager Utility's help system for information on installing a USB license.
Refer to the following topics to get started with USB licenses:
See Also