DL Control Channel Parameters (LTE-Advanced)
The DL Down Link (forward link: from base station to cell phone) Control Channel Parameters dialog contains tabs of settings that allow you to configure the downlink control channel. The following tabs and the corresponding channels are shown below:
- Basic tab: P-SS Primary Synchronization Signal, S-SS Secondary Synchronization Signal, PBCH Physical Broadcast Channel, PCFICH Physical Control Format Indicator Channel, C-RS Cell-specific RS, PDCCH Physical Downlink Control Channel, and PHICH Physical Hybrid ARQ Indicator Channel
- P-RS/MBMS tab: P-RS Positioning Reference Signal, MBSFN-RS Multicast-Broadcast Single Frequency Network Reference Signal, PMCH Physical Multicast Channel
- CSI tab: CSI-RS Channel State Information Reference Signal
See Also