PDCCH Bits (LTE-Advanced)
Mapped
Mapped, Demapped, Deinterleaved, Descrambled, Deratematched, Decoded
specifies how much coding to undo before showing the bits from PDCCH Physical Downlink Control Channel on the CW0/1 Decoded Symbol Tables. See 3GPP TS Technical Specification 36.212, Section 5.3.3 for a diagram of the coding operations performed on PDCCH.
The following is a list of the available selections and the resulting bits shown on the . NREG is the number of resource element groups not allocated for PHICH Physical Hybrid ARQ Indicator Channel or PCFICH Physical Control Format Indicator Channel in a subframe.
-
- raw PDCCH bits are shown on the Symbol Table. No PDCCH bits will be shown in the
-
- NREG * 8 demapped (interleaved) DCI Downlink Control Information format bits for each subframe
-
- NREG * 8 deinterleaved (scrambled) DCI format bits for each subframe
-
- NREG * 8 descrambled (rate-matched) bits for each subframe
-
- S (8 + LENi) bits for each subframe
Each set of bits for an active PDCCH transmission consists of an 8-bit length field (LENi) followed by the deratematched (channel coded) bits.
LENi indicates the number of deratematched bits for the ith PDCCH transmission in a subframe and can be used to determine where a PDCCH ends and the next PDCCH begins in the .
LENi = 3 * (DCI Payload Length + CRC Cyclic Redundancy Check Length)
-
- S (8 + LENi) bits for each subframe
Each set of bits for an active PDCCH transmission consists of an 8-bit length field (LENi), the decoded (DCI payload + CRC) bits, and the 16-bit CRC.
LENi indicates the number of decoded bits (including CRC) for the ith PDCCH transmission in a subframe and can be used to determine where a PDCCH ends and the next PDCCH begins in the .
LENi = DCI Payload Length + CRC Length
For both and PDCCH bits, the LTE Long Term Evolution-Advanced demodulator autodetects the number of active PDCCH transmitted within each subframe, nPDCCH.
The PDCCH decoder is On when RB Auto Detect Mode is set to or when is not set to .
The same PDCCH bits are shown on both and traces to allow marker coupling.
To determine the location of bits for this physical channel in the , use the DemodOFDMSubcarType key in the trace header. This key can be included when saving a trace to disk or can be accessed programmatically from the Trace.MeasurementData.State dictionary.
See Also