Direction (LTE-Advanced)
Downlink
Downlink, Uplink
specifies whether the LTE Long Term Evolution-Advanced signal is an uplink signal or a downlink signal. Changing this parameter will modify the appearance of the LTE-Advanced Demod Properties dialog to show appropriate measurement parameters.
While most parameters can be set differently for each component carrier, this parameter is required to be the same across all component carriers.
In uplink, the IQ traces (IQ Meas, IQ Ref, IQ Meas Time, IQ Ref Time) show a composite of the PUSCH Physical Uplink Shared Channel time domain symbol points and the other channels and signals' frequency domain symbol points. To view PUSCH symbol points in the frequency domain, use the IQ Freq Meas and IQ Freq Ref traces.
See Also