PUSCH DFT Swap (LTE-Advanced)
Cleared
influences how data is mapped to the subcarriers in the Physical Uplink Shared Channel after a discrete Fourier transform is performed. This parameter can be turned on or off to provide two different interpretations of how data should be mapped to resource elements in PUSCH Physical Uplink Shared Channel channels.
See Also