Sync Type (LTE-Advanced)
P-SS Primary Synchronization Signal for downlink
PUSCH Physical Uplink Shared Channel DM-RS DeModulation Reference Signal (LTE) for uplink
C-RS Cell-specific RS for downlink
PUSCH DM directed mesh: The realizations of a physical mesh using substantially directional antennas. See also: mesh-RS, PUCCH Physical Uplink Control Channel DM-RS, S-RS, or PRACH Physical Random Access Channel for uplink
SyncCorr data result in the Error Summary trace.
sets the channel or signal to be used for synchronization. The current selection of is shown to the right of theDownlink
The demodulator can be set to use either the Primary Sync Signal (P-SS) or the cell-specific reference signal (C-RS) to synchronize the downlink signal.
This synchronization is performed at the frame level. For smaller scale adjustments (such as at the symbol or slot level), see the EVM Minimization parameter.
P-SS is normally used for downlink synchronization. However, when P-SS is impaired in some way (for example, P-SS has a different Cell ID than C-RS), C-RS can be used for synchronization so that the signal can be demodulated.
S-SS must be present in the time capture (Raw Main Time) for demodulation to occur, since finding S-SS Secondary Synchronization Signal is the only way to distinguish between the beginning and the middle of a frame.
When
is set to :- The Error Summary data result SyncCorr shows which C-RS antenna port's reference signal was used for synchronization to the right of the correlation value.
- Autodetection of Cell ID and Custom RS-PRS are not supported.
- The reference C-RS port must be specified, since the demodulator does not automatically search the reference measurement channel for all C-RS antenna ports when is set to .
Uplink
The demodulator can use PUSCH DM-RS, PUCCH DM-RS, S-RS, or PRACH for synchronization. Only the channels or signals that are defined for the current user (by selecting the LTE Allocation Editor) will be available as synchronization options.
check box for that signal in thePUSCH, PUCCH, PUSCH DM-RS, PUCCH DM-RS, and SRS Signaling Reference Signal powers in the LTE Allocation Editor are specified relative to the 0 dB level determined by the power of the channel chosen for synchronization.
For example, when:
- is set to
- PUCCH = 3 dB
- PUSCH = 1.2 dB
In this case, the demodulator would set the 0 dB level to be 3 dB below the average power of PUCCH DMRS and would expect PUSCH average power to be 1.2 dB above the 0 dB level, which is equivalent to 1.8 dB below the average PUCCH DMRS power.
LTE Allocation Editor topic for more information about defining a sync slot or click one of the following links for instructions on configuring the sync slot for a particular channel.
also determines which channel's parameter is used for frame boundary calculation. See theSee Also