SyncCorr (LTE-Advanced)
shows the amount of correlation between the measured synchronization signal and the ideal synchronization signal. The correlation is expressed as a percentage of the ideal synchronization signal autocorrelation magnitude.
also shows the synchronization signal used for synchronization. For downlink, the synchronization signal is either P-SS or C-RS. For uplink, the synchronization signal is PUSCH DMRS, PUCCH DMRS, SRS, or PRACH. The Sync Type parameter determines the channel or signal that is used for synchronization.
In addition, for downlink signals, shows which C-RS Cell-specific RS antenna port was used for synchronization when Sync Type is set to .
See Also