PUSCH (LTE-Advanced)
(Physical Uplink Shared Channel) contains uplink user data.
When is selected, Frame Summary will show a PUSCH Physical Uplink Shared Channel group named for each modulation type under .
When is cleared, will show the PUSCH information in the row for the uplink user currently selected for analysis. The other user's rows will show "---" since the demodulator can only analyze one user at a time.
Uplink user allocations can be defined in the LTE Allocation Editor.
This channel's SC-FDMA Single Carrier - Frequency Division Multiple Access modulation type will be displayed as QPSK Quadrature phase shift keying, 16QAM, QAM64, QAM256 (only available when Enable Higher Order Modulation or Enable 1024 QAM is selected), or QAM1024 (only available when Enable 1024 QAM is selected). when the PUSCH channel contains a single modulation type. When PUSCH contains a combination of modulation types, will display "---".
See Also