TDD Ack/Nack Feedback Mode (LTE)
Multiplexing
Multiplexing, Bundling
determines which HARQ Hybrid Automatic Repeat Request Ack/Nack feedback mode is used. The following selections are available:
See 3GPP TS Technical Specification 36.212, Section 5.2.2.6 and 3GPP TS 36.213, Section 7.3 for more information about TDD Time Division Duplex: A duplexing technique dividing a radio channel in time to allow downlink operation during part of the frame period and uplink operation in the remainder of the frame period. Ack/Nack feedback mode.
See Also