Decode Tab (LTE)

Menu Path: Analysis > LTE Demod Properties... > Decode tab

The Decode tab of the LTE Demod Properties dialog box allows you to specify what level of channel decoding to perform as well as specify other parameters needed for information decoding for the DL Decode Info and UL Decode Info summary tables. The decoded bits are shown on the Decoded Symbol Table (uplink) and the CW 0/1 Decoded Symbol Tables (downlink).

There are two different versions of the Decode tab, one for downlink and one for uplink signals.

Downlink parameters

The parameters for the downlink version of the Decode tab are listed below (click on a parameter for more information).

Uplink parameters

The parameters for the uplink version of the Decode tab are listed below (click on a parameter for more information).

See Also

5G Candidate Tab

Advanced tab

Format Tab

Profile Tab

Time Tab

LTE Demod Properties Dialog Box