Bandwidth (LTE)
sets the LTE Long Term Evolution signal bandwidth (which also determines the total number of resource blocks). Below is a list of available bandwidths:
|
Available Bandwidths |
|---|
| 1.4 MHz Megahertz: A unit of frequency equal to one million hertz or cycles per second. (6 RB Resource Block) |
| 3 MHz (15 RB) |
| 5 MHz (25 RB) |
| 10 MHz (50 RB) |
| 15 MHz (75 RB) |
| 20 MHz (100 RB) |
See Also