Dw/GP/Up Len (LTE)
0
0-8
specifies which special subframe configuration is being used in an LTE Long Term Evolution TDD Time Division Duplex: A duplexing technique dividing a radio channel in time to allow downlink operation during part of the frame period and uplink operation in the remainder of the frame period. signal. There are nine special subframe configurations for Normal CP length and seven special subframe configurations for Extended CP length. These configurations are listed in Table 4.2-1 in 3GPP TS Technical Specification 36.211.
This parameter only applies to LTE Frame Type 2 TDD signals and is only present on the Format tab when Duplex Mode is set to .
See Also