Edit Rate Match Pattern... (LTE)

Edit Rate Match Pattern... opens the LTE Downlink Rate Match Pattern dialog, which allows you to configure up to eight rate match patterns applied to any PDSCH Physical Downlink Shared Channel allocation.

This feature can be used to configure O-RAN Radio Access Network Fronthaul WG4 rate match patterns that puncture (mask) specific resource elements (REs) during PDSCH demodulation, in accordance with O-RAN.WG4.TS Technical Specification.CUS.0 section 7.5.3.5.

A resource element is masked (treated as "missing" — zero in the U-Plane, and excluded from demodulation, EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format., and decoding) only where all of the following select it at once within a given rate match pattern:

Note that enabling a newly added Rate Match pattern, and leaving every other parameter at its default value has no effect. This is due to the Symbol Bitmap default value being all-zero’s, so no symbols are masked by default. Remember to configure the correct combination of Time Parameters (Slot Pattern Periodicity, Slot Pattern Bitmap, Symbol Bitmap) along with Frequency Parameters (RB Bitmap Index, RE Mask Bitmap) in order to specify the desired rate matching patterns.

Parameters

Rate Match - Selects a rate match pattern ID for editing. There is a single rate match pattern (0) by default. Use this parameter along with Add Rate Match, Remove Rate Match and Clear All to manage multiple rate match patterns.

Default: 0

Enabled - Enables or disables the selected Rate Match pattern ID. When cleared, no resource elements are masked by that Rate Match pattern ID.

ID - Sets a numerical identifier for the selected Rate Match pattern. The ID is automatically assigned when a new Rate Match pattern is added as the lowest available ID value in the 0-7 range of possible IDs.

Default: 0

Range: 0 - 7

Time Parameters

Slot Pattern Periodicity - sets the length, in LTE Long Term Evolution slots, of the repeating window over which Slot Pattern Bitmap applies. One LTE slot is 0.5 ms and contains 7 OFDM symbols (normal cyclic prefix) or 6 OFDM symbols (extended cyclic prefix).

Default: N1

Choices: N1, N2, N4, N5, N8, N10, N20 (cycle length of 1, 2, 4, 5, 8, 10, or 20 slots)

Slot Pattern Bitmap - a binary string, one bit per slot within the Slot Pattern Periodicity window (leftmost bit = first slot of the window), selecting which slots within the repeating slot pattern period has the active rate match pattern applied. A bit value of 1 means the rate match pattern is active during that slot; 0 means it is inactive.

Default: all 1s (active every slot)

Symbol Bitmap - a binary string of 7 bits, one bit per symbol (only the first 6bits are used for extended cyclic prefix; the 7th bit is ignored), leftmost bit = symbol 0, selecting which OFDM symbols within a selected slot (as determined by Slot Pattern Bitmap) has the active rate match pattern applied. A bit value of 1 means the rate match pattern is active during that symbol; 0 means it is inactive.

Default: all 0s (no symbols selected)

Frequency Parameters

RB Bitmap Index - selects which frequency PRBs the rate match pattern applies to, entered as a comma-separated list of PRB indices or ranges (for example, 1:5 selects PRBs 1 through 5). PRB 0 is the lowest-frequency PRB in the current analysis bandwidth. Type directly into the field, or double-click to open an edit dialog.

Default: all PRBs selected for the current analysis Bandwidth

RE Mask Bitmap - a 12-bit binary string, one bit per resource element (leftmost bit = RE0, the lowest-frequency RE in the PRB; rightmost bit = RE11) within a selected PRB (as determined by RB Bitmap Index). A bit value of 1 means PDSCH data is transmitted in that RE; 0 means the RE is masked (punctured).

Default: all 0s (every RE is punctured)

Example

Consider a 10 MHz Megahertz: A unit of frequency equal to one million hertz or cycles per second., 100 PRBs, normal cyclic prefix test signal. The O-RAN Fronthaul WG4 LTE reMask conformance test (O-RAN.WG4.TS.CONF.0-R005-v15.00 section 3.2.3.7.4) specifies puncturing of every odd-indexed RE on PRBs 1-5 of symbol index 6 within the first slot index of each subframe, with all other PRBs within symbol index 6 inactive. For this test case we can configure:

Rate Match ID: 0

Rate Match ID: 1

Rate Match Pattern is supported for downlink only, and configures one component carrier at a time; on LTE-A carriers, open Edit Rate Match Pattern... from each component carrier's own Profile(CCx) tab to configure that carrier's pattern independently.

See Also

Profile Tab

EVM

LTE Demod Properties Dialog Box