RSSI (LTE)
(Received Signal Strength Indicator) is defined as the average power for all symbols containing C-RS Cell-specific RS from antenna port 0. is calculated from symbols in the Measurement Interval.
When there are multiple measurement channels present that contain transmissions from C-RS antenna port 0, the average symbol power is calculated for each measurement channel individually and added together to compute.
See Also