Freq Err Per Slot (LTE)
shows the frequency error of the signal as a function of slot number for the data in the Measurement Interval. This is the frequency error that is compensated on a per-slot basis as part of the EVM minimization process.
The frequency error is expressed as an offset in Hz from the current center frequency setting.
See Also