ChEstCorrMin (MB-OFDM)
ChEstCorrMin (Channel Estimation Correlation Minimum) gives the minimum correlation between the measured Channel Estimation Sequence portion of the Preamble and the ideal Channel Estimation Sequence. The ChanEstCorr (Channel Estimation Correlation) is computed on a symbol by symbol basis so the ChEstCorMin is the lowest of these individual symbol correlations. The result shows both the value at this symbol expressed in percentage and the location of the symbol. A value of 100% indicates perfect correlation and a value of 0 indicates no correlation.
See Also