Band Centered FFI Analysis (MB-OFDM)
Depends
on Preset to Standard selection
For TFC Transport Format Combination Auto: Clear
For manual TFC (by specific TFC and channel): Selected
(See MB-OFDM Standard Setups/Presets Table.)
When the checkbox is selected, the must be set to the center of the FFI band being analyzed, which is different from the center frequency for TFC5 and TFC7.
When cleared, the needs to be set to the center frequency for all TFCs. This allows automatic detection of any TFC in the band group without having to change the center frequency.
See Also