Using Standard Setups/Presets  (MB-OFDM)

Menu Path: Analysis > MB-OFDM Demod Properties > Format tab > Preset to Standard button

The Preset to Standard button selects an MB-OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. standard preset configuration based on a Band Group 1 - 6 and the Time-Frequency Codes (TFC Transport Format Combination) associated with that band group.

The preset conditions are listed below:

Parameter

Value

Auto CPE Filter Length

Set by TFC selection (auto or channel).

Band Centered FFI Analysis

Set by TFC selection (auto or channel).

Band Group

Band Group value selected.

Center Frequency

Determined by TFC selection (auto or channel).

Data Rate Auto

Selected

Data Rate (inactive)

53.3Mb/s

Frequency Hopping Analysis

Select

Frequency Span

0.6/1.65 GHz Gigahertz: A frequency measurement which equals one billion hertz. (FFI/TFI)

Normalize IQ Traces

Select

Manual Override - Result Length (inactive)

108 symbol-times

Max Result Length

108 symbol-times

Measurement Interval

108 symbol-times

Measurement Offset

0 symbol-times

Mirror Frequency Spectrum

Clear

Packet Avg RBW Resolution Band Width (RBW or ResBW): specifies the minimum frequency bandwith that two separate frequency spectra can be resolved and viewed seperately. For FFT (digital) based VSA's the process is equivalent to passing a time-domain signal through a bank of bandpass filters, whose center frequencies correspond to the frequencies of the FFT bins. For a traditional swept-tuned (non-digital) spectrum analyzer, the resolution bandwidth is the bandwidth of the IF filter which determines the selectivity.

5 MHz Megahertz: A unit of frequency equal to one million hertz or cycles per second.

Payload Octets

0

Phase Track Average Length

4 (TFC 1 to 4), 12 (TFC 5 to 7), 6 (TFC 8 to 10)

Post-Packet Time

0 symbol-times

Post-Symbol Time

0.194 symbol-times

Preamble Type

Auto

Pre-Packet Time

0 symbol-times

Pre-Symbol Time

0 symbol-times

Pulse Search

Select

Result Length

From Header

Search Length

100uSec

Show Filtered CPE

Clear

Subcarrier Select

All

Symbol Gate Length

160 clocks

Symbol Timing Adjust

-1 clocks

Time Frequency Code

Value you select with the Preset to Standard button

Time Scale Factor

1

See Also

MB-OFDM Modulation Overview

MB-OFDM Demod  Properties Dialog Box

Format Tab (MB-OFDM Demod Properties)

Time Tab (MB-OFDM Demod Properties)

Packet Tab (MB-OFDM Demod Properties)

Advanced Tab (MB-OFDM Demod Properties)