Advanced Tab  (MB-OFDM)

Menu Path: Analysis > MB-OFDM Demod Properties > Advanced tab

The Advanced tab accesses advanced parameters used to demodulate nonstandard and/or user defined MB-OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. signals and to manipulate trace data results. Click on a parameter link for specific parameter information.

See Also

Format Tab (MB-OFDM Demod Properties)

Time Tab (MB-OFDM Demod Properties)

Packet Tab (MB-OFDM Demod Properties)