Symbol Gate Length (MB-OFDM)
160 clocks (See MB-OFDM Standard Setups/Presets Table.)
128 - 165 clocks
determines the length of the symbol gate for each symbol in a particular band thus defining the end of the time gate relative to the end of the 128 IFFT Inverse Fast Fourier Transform samples of that symbol. This is an alternative to the entry for test specification where the starting point varies but the symbol gate length needs to remain constant. When the is set, changing the will change the in order to leave the the same. Changing the will change the , and vice versa, keeping the constant. See Pre-Symbol Time and Post-Symbol Time for more information.
See Also