ChanEst Pwr - Packet Summary (MB-OFDM)
ChanEst Pwr (Channel Estimation Power) is the absolute power in the Channel Estimation section (6 symbols) of the current MB-OFDM Packet preamble averaged over all bands and computed in dBm deciBels referenced to a milliWatt: dB relative to 1 milliwatt dissipated in the nominal input impedance of the analyzer.
See Also
ChanEst Pwr - Band Packet Summary Table (MB-OFDM)