Hdr Pwr - Packet Summary (MB-OFDM)
Header Power is the absolute power in the Header section of the current MB-OFDM Packet averaged over all bands and computed in dBm deciBels referenced to a milliWatt: dB relative to 1 milliwatt dissipated in the nominal input impedance of the analyzer.
See Also
Hdr Pwr - Band Packet Summary Table (MB-OFDM)