Overall EVM - Packet Summary (MB-OFDM)
Overall EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format. (Error Vector Magnitude) is the RMS level of the Error Vector Magnitude in the header and payload part of the MB-OFDM Packet averaged over all bands and computed in %rms.
See Also
Overall EVM - Band Packet Summary Table (MB-OFDM)