Packet Pwr - Packet Summary (MB-OFDM)
Packet Power is the absolute power in the overall MB-OFDM Packet averaged over all bands and computed in dBm deciBels referenced to a milliWatt: dB relative to 1 milliwatt dissipated in the nominal input impedance of the analyzer.
See Also
Packet Pwr - Band Packet Summary Table (MB-OFDM)
Available Packet Summary Data (MB-OFDM)
Packet Summary Table (MB-OFDM)