Pyld Pwr - Packet Summary (MB-OFDM)
Payload Power is the absolute power in the Payload section of the current MB-OFDM Packet averaged over all bands and computed in dBm deciBels referenced to a milliWatt: dB relative to 1 milliwatt dissipated in the nominal input impedance of the analyzer.
See Also
Pyld Pwr - Band Packet Summary Table (MB-OFDM)