About NB-IoT Modulation Analysis

89601BHTC (89601B-BHT) adds NB-IoT modulation analysis capability to your 89600 VSA software.

With 89601BHTC (89601B-BHT) NB-IoT Modulation Analysis, you can demodulate signals that conform to the following standards:

With the NB-IoT demodulator, you can demodulate downlink and uplink signals. Once required parameters are specified, the demodulator will automatically lock onto the signal. The demodulator can perform power-based autodetection of NPDSCH and NPUSCH allocations for signals.

The demodulator provides various signal analysis capabilities including decoded bits, EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format. calculations, IQ constellation, channel equalization data, and error summary data. Flexible display scaling and marker functionality enhance these measurement capabilities.

For more information about supported reference signals, control channels, and transport channels see the Available Features topic.

See Also

Available Features

Setting up an NB-IoT Measurement

Selecting NB-IoT Demodulation

Troubleshooting