RB Auto Detect Mode (NB-IoT)
Power Based
selects the method used to determine valid NPDSCH RB allocations to be measured.
-
- RB autodetection is disabled.
-
- allocations are autodetected based on the power level of the NPDSCH/NPUSCH transmissions and which subframes are assigned to NPDSCH/NPUSCH. Use Power Det. Threshold to set the threshold for power-based detection.
See Also