Selecting NB-IoT Demodulation
Configures the 89600 VSA to demodulate NB-IoT signals (downlink) that are compliant with the 3GPP Technical Specifications listed in About Option BHT: NB-IoT Modulation Analysis.
After selecting the NB-IoT demodulator, the measurement configuration parameters must be configured. You can use Preset to set parameters to typical values, or you can configure the VSA manually from the NB-IoT Demod Properties dialog box.
Reviewing the Setting up an NB-IoT Measurement topic is also recommended.
Configure the demodulator
After selecting the NB-IoT measurement type, you need to set certain configuration parameters on the tab of the NB-IoT Demod Properties dialog box to ensure demodulation of your signal. For a detailed setup procedure, see Setting up an NB-IoT Measurement.
Example recordings
The 89600 VSA includes several example NB-IoT signals that can be used to help you learn how to use the NB-IoT demodulator. The included signals are listed in the Demo and Recorded Signals topic in the Getting Started book.
See Also