NPUSCH All Symbols Transmitted (NB-IoT)
Enabled
determines whether NPUSCH is transmitted during E-UTRA UMTS Terrestrial Radio Access: A W-CDMA standard developed ETSI, ARIB and the TIA. This system uses DSSS and either FDD or TDD depending on its frequency assignment and application. SRS signal. This parameter is only available when Operation Mode is set to In-band.
When enabled (selected), all NB-IoT symbols for NPUSCH are transmitted.
When disabled, the resource elements in SC-FDMA Frequency Division Multiple Access: Method of allowing multiple users to share the radio frequency spectrum by assigning each active user an individual frequency channel. In this practice, users are dynamically allocated a group of frequencies so that the apparent availability is greater than the number of channels. symbols overlapped with a symbol configured with SRS according to SRS Subframe Configuration shall be counted in the NPUSCH mapping, but these resource elements are not used for transmission of the NPUSCH.
See 3GPP TS Technical Specification 36.211 10.1.3.6 and 36.331 6.7.3.2 for more information.
See Also