Auto (N-TM Signal) (NB-IoT)
Disabled
The checkbox enables the NB-IoT demodulator to autodetect whether the signal is an N-TM (narrowband test model) signal.
-
- When enabled, the demodulator will automatically determine whether the signal is an N-TM signal. When this parameter is enabled, a minimum of 8 frames of data will be acquired to detect the signal type.
-
- When disabled, the demodulator will use the N-TM Signal parameter to determine whether the signal is an N-TM signal.
See Also