N-TM Signal (NB-IoT)
False
The parameter determines if the signal is an N-TM (narrowband test model) signal. This parameter is visible only when RB Auto Detect Mode is set to Power-based.
-
- When false, the demodulator will assume the signal is not an N-TM signal.
-
- When true, the demodulator will assume the signal is an N-TM signal. A minimum of 8 frames of data will be acquired and Subframe 19 channel type will be assumed to be NSSS.
This parameter is ignored when Auto N-TM signal detection is enabled.
See Also