Power Detection Threshold (NB-IoT)
-15 dB
-100 to 100 dB
sets the threshold for RB power detection mode when RB Auto Detect Mode is set to Power-based. If the threshold is -15dB, all RBs whose power is higher than 15 dB below NRS power are detected as active.
See Also