N-TM Signal (NB-IoT)
displays true if the signal is an N-TM (narrowband test model) signal and false if the signal is not N-TM.
For more information, see the N-TM Signal measurement parameter.
See Also
displays true if the signal is an N-TM (narrowband test model) signal and false if the signal is not N-TM.
For more information, see the N-TM Signal measurement parameter.
See Also
|
Copyright © 2000-2026 Keysight Technologies, Inc. |