RSSI (NB-IoT)
(Received Signal Strength Indicator) is defined as the average power for all symbols containing NRS from antenna port 0. is calculated from symbols in the Measurement Interval.
See Also
(Received Signal Strength Indicator) is defined as the average power for all symbols containing NRS from antenna port 0. is calculated from symbols in the Measurement Interval.
See Also
|
Copyright © 2000-2026 Keysight Technologies, Inc. |