Available Summary Tables (NB-IoT)
NB-IoT modulation analysis provides the following summary tables:
- Decoded Symbol Table - shows the decoded bits from NPUSCH and NPUCCH.
- DL Decode Info - shows the decoded data from NPBCH and NPDSCH.
- Error Summary - provides information about the quality of the signal being analyzed.
- Frame Summary - provides EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format., power, modulation type, and number of resource blocks occupied for the channels and signals that are present.
- MIMO Info Table - lists information about NRS/Rx paths present in the signal. This information is calculated from the narrowband cell-specific reference signal.
- Symbol Table - shows the symbol values of the subcarriers before decoding.
- UL Decode Info - shows the decoded data from NPUSCH.
See Also