SymClk Err (NB-IoT)
shows the frequency error between the measured signal's symbol clock and the reference symbol clock in parts-per-million (ppm). The error is calculated by averaging the symbol timing corrections during the Measurement Interval.
A value of 0.010 ppm indicates that the measured signal's symbol clock frequency is slower than the reference symbol clock frequency by 0.000 000 01 * RefSymClk.
See Also