SyncCorr (NB-IoT)
shows the amount of correlation between the measured synchronization signal and the ideal synchronization signal. The correlation is expressed as a percentage of the reference synchronization signal autocorrelation magnitude.
also shows the synchronization signal used for synchronization. For downlink, the synchronization signal is NPSS. For uplink, the synchronization signal is NPUSCH-DMRS or NPRACH itself.
See Also