Time Offset (NB-IoT)
shows the time offset from the beginning of the time capture to the beginning of the Measurement Interval.
For example, when = 5 ms and the Search Time trace starts at -8.3 ms, the beginning of the is located at -3.3 ms within the trace.
can be used to measure the accuracy of an external frame trigger signal when
- a frame trigger signal is connected to the external trigger
- Analysis Start Boundary is set to Frame
- and Measurement Offset is set to 0
In this case, will show the offset between the frame trigger and the actual start of the frame.
See Also