NSSS (NB-IoT)
NSSS is the Secondary Synchronization signal for an NB-IoT downlink frame.
See Downlink Control Channel Properties for information on setting NSSS .
NSSS is transmitted as a Zadoff-Chu sequence and thus appears as irregularly spaced points on a circle in the IQ Meas constellation diagram.
NPSS and NSSS can be transmitted on a single NRS antenna port or all of them together.
See Also