RSCTE (NB-IoT)
shows the average magnitude of the common tracking error calculated from the narrowband reference signal for each NRS/Rx path. is computed by calculating the common tracking error for the NRS subcarriers and then rms averaging the errors.
is calculated from the data in the Measurement Interval.
is expressed as a percentage of the ideal signal, which has a common tracking error of 1. See the Common Tracking Error trace topic for more information.
is calculated with a Symbol Timing Adjust setting of . When is set to a value other than , may not match the corresponding Common Tracking Error data results in the Error Summary table and Common Tracking Error trace.
See Also