Decoded Symbol Table (NB-IoT)
shows the decoded bits for the physical layer channels NPBCH and NPDSCH.
The level of decoding is determined by the parameters on the Decode Tab.
The default bit order for this trace is MSB Most significant bit. In a binary coding scheme, the bit having the greatest numerical value. Analogous to the left-most numeric position in a decimal number.-first.
See Also