Auto Set Span (5G NR/5G-Advanced)
Default: Disabled (cleared)
Auto Set Span - Enables or disables whether measurement span is coupled to provide minimal sample rate required by maximum Transmission Bandwidth of the primary component carrier. If enabled, span is automatically coupled to provide a sample rate to minimize data size and resampling overhead. If disabled, span is set manually by use.
If value is true, the Spectrum trace may not include full visibility of the signal bandwidth.
See Also