MIMO Condition Number (5G NR/5G-Advanced)
sets the controls for condition number calculations.
Control - Selects the unit used to calculate the condition number vector displayed in the MIMO Condition Number trace.
Off - (default) Turns off condition number calculations.
Per Subcarrier - Calculates the condition number for each subcarrier.
User Defined RBs - Calculates the condition number per user-defined number of RBs.
Wideband - Calculates a single condition number for the entire PUSCH bandwidth.
RB Granularity - If User Defined RBs is selected, condition number is averaged over the number of RBs set in the RB Granularity field.
Default: 1
See Also