Report EVM in dB (5G NR/5G-Advanced)
Default: Disabled (cleared)
Report EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format. in dB specifies the EVM units for all traces.
When selected, EVM will be reported in dB.
When cleared, EVM will be reported in %rms.
The reference for EVM calculation in both cases are the ideal IQ points which are shown on the IQ Ref trace.
See Also