IQ Gain Imbalance (5G NR/5G-Advanced)
indicates the amount of amplifier gain imbalance between I and Q. For example, a value of -6.02 dB means the Q signal is being amplified twice as much as the I signal. This measurement is expressed in dB and calculated over the data in the measurement interval.
See Also