IQ Quad. Error (5G NR/5G-Advanced)
(IQ quadrature error) indicates the amount of the angle skew between the I and Q signals for the data in the measurement interval. Ideally, I and Q should be 90 degrees apart. An IQ quadrature error of -300 mdeg means that I and Q are actually 89.7 degrees apart.
See Also