Beam Pattern Summary (5G NR/5G-Advanced)
There are two types of traces in the Trace > Data > Demod and MIMO Multiple Input, Multiple Output: A physical layer (PHY) configuration in which both transmitter and receiver use multiple antennas. menus that display component carrier data: CCn (component carrier is fixed), and Selected Display CC (component carrier is dynamically selected using the Display parameter). See About Per-Carrier Trace Types for more information.
This table summarizes the beam peaks of all users on all layers in all antenna groups per physical channel.
Labels
Name - Each beam is assigned a name by the VSA software based on the physical channel(s) selected and other settings in the Beam Patterns Include parameter group. Physical channels include:
SSB - SSBn_Periodn_Blockn
PDSCH Physical Downlink Shared Channel - PDSCHn_Layern
PUSCH - PUSCHn_Layern
CSI channel state information-RS - CSI-RSn_Portn
Physical Channel - (default: not visible) Identifies the physical channel included in the beam.
User - (default: not visible) Identifies the user for each beam.
PeriodIndex - (default: not visible) Identifies the period index for each beam.
Layer - (default: not visible) Identifies the beam's layer number.
AntennaGroupIndex - (default: not visible) Identifies the beam's antenna group index.
Metrics
Azimuth Peak (deg) - Displays the beam's azimuth angle.
Elevation Peak (deg) - Displays the beam's elevation angle.
Azimuth Width (deg) - Displays the beam's angle width in the azimuth plane.
Elevation Width (deg) - ) Displays the beam's angle width in the elevation plane.
Peak Power per RE (dBm deciBels referenced to a milliWatt: dB relative to 1 milliwatt dissipated in the nominal input impedance of the analyzer) - Displays the absolute power in dBm of the current lobe peak.
Peak Power per RE (dB) - Displays the peak power in dB, relative to the total power of the corresponding layer or SSB block (port). The Portn Peak Power(dB) = Portn Beam Peak Power(dBm) – Portn_TotalPower.
In releases earlier than 29.40, Peak Power (dB) was measured relative to the maximum Beam Peak Power of all layers and SSB blocks, resulting in a much higher value.
See Also