About Symbol Table (5G NR/5G-Advanced)

Symbol Table shows the numerical values of demodulated data (the data in the Measurement Interval) for the selected layer.

The numerical values can be shown as hexadecimal or binary digits. The default is hexadecimal and the Symbol Table Format selection (i.e. to select Binary) is under Trace > Properties > Digital Demod.

This trace has the following characteristics:

To view decoded channel information bits, use the Decoded Symbols Table.

See Also

About Frame Summary

PHICH bit mapping