Frame Summary (5G NR/5G-Advanced)
There are two types of traces in the Trace > Data > Demod and MIMO Multiple Input, Multiple Output: A physical layer (PHY) configuration in which both transmitter and receiver use multiple antennas. menus that display component carrier data: CCn (component carrier is fixed), and Selected Display CC (component carrier is dynamically selected using the Display parameter). See About Per-Carrier Trace Types for more information.
The trace shows the reference component carrier's EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format., power, modulation format, number of resource blocks occupied and RNTI for the channels that are present in the Measurement Interval.
Frame Summary is a type of Matrix Table that provides sortable rows by column, selectable column visibility, and copy/paste and export functionality to share rows of content or complete tables to applications like email, text editing or spreadsheet programs.
|
Not visible by default To make visible, right-click any column heading and select Column Visibility... |
|||||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
| Name | Physical Channel | User | Part | Layer | EVM (%rms) | SINR Signal to (Interference + Noise) ratio (dB) | Power per RE (dBm deciBels referenced to a milliWatt: dB relative to 1 milliwatt dissipated in the nominal input impedance of the analyzer) | Modulation | Num. of RBs | RNTI | BWP ID | PID | Time Advance (ns) |
|
Name is a unique, but arbitrary reference to a Frame Summary row that is derived from Physical Channel, User, Part and Layer as applicable. Possible names include: Downlink:
Uplink:
|
Physical channels include:
|
When there is a single user, the default user number is 0. Rows without user data are denoted with '***'. |
Some physical channels have multiple parts. Physical channel parts include:
(0) Data (1) DMRS (2) PTRS |
Rows without layer data are denoted with '***'. |
EVM is the per-layer RMS EVM after demodulation. The Report EVM in dB parameter affects the units of this data result.
NOTE: When PUCCH0 and PUCCH1 have overlapping resources (see Sequence Cyclic Shift), EVM result will only be shown on PUCCH1, and it will be the composite EVM of both PUCCH0 and PUCCH1. |
SINR is the signal-to-noise and interference ratio for the channel. |
Power per RE is the per-subcarrier power received at the reference measurement channel, averaged over all the subcarriers belonging to the physical channel. |
Modulation is the modulation format of the channel. The modulation format for Non-alloc signals is not shown.
BPSK_45Deg QPSK Quadrature phase shift keying QAM16 QAM64 QAM256 BPSK_PI/2 Z-Chu |
Num. of RBs shows the number of resource blocks (1 RB x 1 slot) within the Measurement Interval that contain subcarriers belonging to the channel. Num. RB is not shown for Non-alloc signals. |
RNTI shows the Radio Network Temporary Identifier (RNTI)for the channel. |
BWP ID displays the ID number of the BWP that is associated with the row's physical channel. |
PID displays the auto-detected Preamble ID. PID is only available in PRACH Physical Random Access Channel Auto Detection mode. If '***' is displayed, make sure that PRACH Auto Detection is enabled. |
Time Advance displays the auto-detected timing offset. When doing the Time Advance measurement, the assumption is the signal is captured using frame trigger, and the Time Advance is the difference between the actual PRACH Occasion time relative to the frame boundary and the expected PRACH Occasion Time relative to the frame boundary. When PRACH TA Relative to Trigger is enabled, the PRACH Time Advance results are relative to the trigger instead of the frame boundary. Time Advance is only available in PRACH Auto Detection mode. If '***' is displayed, make sure that PRACH Auto Detection is enabled. |
Averaging is not applied to the Frame Summary trace.
Trace Color coding Scheme
A multi-color coding scheme is used to make it easy to visually identify common symbols, subcarriers, and data results within various OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. Traces. This makes cross trace data comparisons and analysis easier to accomplish. Different colors are assigned to symbols representing elements including: PSS/SSS/PBCH/PBCH_DMRS/PDSCH/PDSCH_DMRS/PUSCH/PUSCH_DMRS/PUCCH/PUCCH_DMRS. Some common color scheme Traces include: Error Vector Spectrum, Error Vector Time, OFDM Meas, Frame Summary and Slot Summary trace data.
The 5G NR color scheme has been simplified to help make visual sense of a complex standard. The default color assignment for 5G NR follows these general guidelines:
- DMRS and PTRS signals
- PTRS and DMRS signals generally are generally assigned cooler colors (greens, blues).
- All DMRS signals share a common color. You can distinguish between DMRS signals using markers, but each DMRS is also visually distinguished by the physical channel in which it is located.
- All PTRS signals share a common color. You can distinguish between PTRS signals using markers, but each PTRS is also visually distinguished by the physical channel in which it is located.
- Physical channels (PDCCH, PDSCH, PUCCH, PUSCH, etc.)
- Physical channels are generally assigned warmer colors (yellows, oranges, reds)
- Each physical channel type has an assigned group of colors. For channel collections (multiple channels of the same type), the display will rotate through a group of three similar but distinct colors to distinguish between each channel in the collection. For example, if a signal contains 6 PDSCHs (PDSCH0-5), PDSCH0, PDSCH1 and PDSCH2 will each have similar but uniquely different color assignments. The same colors will be repeated for PDSCH3, PDSCH4 and PDSCH5.
You can also customize and re-assign Trace colors schemes, see the Display Preferences Color tab (click tab and select a new color for the active Mod Type element).
See Also