Input Extensions (Infiniium)

Input Extensions are the hardware configuration and setup parameters that apply to the Keysight 89600 VSA with Keysight Infiniium Series Oscilloscopes.

To modify a hardware parameter, open the Input Extension dialog (Acquisition > Extended Settings tab), click the parameter name and specify the value. For True/False values, a selected check box sets the value to True. A cleared check box sets the value to False.

Click Preset All to preset all input extension parameters across all logical instruments and channels.

Hardware Configuration Parameters

Parameter 

Value 

Default

CustomTrigCommand

String

<blank>

CustomTrigType

True / False

False

ExternalMixerLoAddress

String

<blank>

Hardware DDC Sample Rate

Double

NaN (when DDC is not active)

Hardware DDC Status

NotApplied / Ddc / HighResolution

NotApplied

RealEdge (High Bandwidth)

Off / On

Off

ResampleLocation

Driver / Measurement

Driver

SampleMode

FullRate / FullRateDdc / Minimize / UserRate

FullRate; FullRateDdc if hardware-based DDC is supported

Sample Rate Actual

Double

NaN

UserSampleRate

Real

1E+09

UserSCPIPreset

String

<blank>


CustomTrigCommand

CustomTrigCommand is used to set trigger parameters on the Infiniium Series Oscilloscopes that cannot be set directly from the 89600 user interface. This parameter enables the user to take advantage of the Infiniium Series scopes extensive trigger conditioning and pattern capability.

A sequence of SCPI commands can be entered, beginning with ":TRIG" and separated by semicolons, into the CustomTrigCommand dialog box. The commands will be transmitted to the scope when the Configure dialog box is closed when the CustomTrigType is set to True. The trigger type selected in the Trigger tab of the Input Properties dialog box (Acquisition > Trigger) is overridden when the commands are transmitted. SCPI Query commands are not supported.

CustomTrigType

When CustomTrigType is true, the trigger types can be configured by entering SCPI commands in the CustomTrigCommand hardware parameter. When this parameter is false, the trigger type is specified in the 89600 software (Acquisition > Trigger tab).

ExternalMixerLoAddress

ExternalMixerLoAddress sets the LAN Local Area Network: A communications network that serves users within a local geographical area, typically over distances of around 100m. Wireless LANs use wireless communicaitons to network devices so there is no need for data cabling. or USB address of the LO address for external mixer configuration. The LAN or USB address of the LO for the system (such as an MXG-B) can be copied from the Keysight Connection Expert on the scope, and pasted here. Please see the External Mixer Connectivity with Infiniium Oscilloscope topic for more details.

Hardware DDC Sample Rate

Hardware DDC Sample Rate displays a read only value and is only available for oscilloscope models with hardware DDC.

When the DDC is active, this field will show the DDC sample rate.

When the DDC is not active, this field will show NaN.

Hardware DDC Status

Hardware DDC Status displays a read only value and is only available for oscilloscope models with hardware DDC.

When oscilloscope Spectrum Analysis (DDC) is active for hardware digital downconversion, this field will show DDC applied.

When oscilloscope High Resolution acquisition mode is active for hardware digital downconversion, this field will show High Resolution applied.

When hardware digital downconversion is not active, this field will show Not applied. Hardware digital downconversion is not applied if the oscilloscope does not have the necessary options present, FullRateDdc is not the selected sample mode, frequency limits are not met, the channel is a differential channel, or the instrument is simulated.

RealEdge (High Bandwidth)

The RealEdge (High Bandwidth) (default: OFF) parameter is used to select the scope Real Edge inputs. The Real Edge inputs can only be switched ON for scopes that support Real Edge inputs and the VSA Logical Channel configuration is set to use scope inputs 1 and/or 3. When HighBandwidthMode is set to OFF then oscilloscope inputs 1 thru 4 will be used. When HighBandwidthMode is set to ON, the scope Real Edge inputs are used.

Real Edge (High Bandwidth) VSA
Logical Ch's
Scope
Inputs 1 thru 4

Scope
Real Edge Inputs

Cleared (OFF) 1 thru 4 1 thru 4 OFF
Selected (ON) 1 thru 2 OFF ON

ResampleLocation

The 89600 VSA software automatically resamples the scope input data to satisfy the data sample requirements for the current VSA measurement span. This minimizes the amount of data required and used for a particular measurement. The large data capture memory size capability of the Infiniium series oscilloscopes can exceed the 89600 VSA software internal data limit. The "ResampleLocation" parameter takes advantage of these longer time lengths by resampling in the 89600 software's driver for the Infiniium scopes (this occurs before the 89600 measurement system block). For more information on resampling and VSA theory of operation, see Application Note 150-15 Keysight Vector Signal Analysis Basics (see Product Literature). There are two ResampleLocation modes: Measurement mode and Driver (default) mode:

Measurement mode:  

When ResampleLocation is set to Measurement, the resampling of the input time data is implemented in the 89600 VSA "Measurement" system block which bypasses the "Driver" digital decimating filter system block, see the following VSA system block diagram. In "Measurement" mode, the current measurement is limited to 8.2 M pts of the scope input data. This in turn limits the VSA maximum time Record Length and either the Search Length or Result Length depending on the type of measurement.

"Measurement" mode limits the current VSA measurement to 8.2 M pts of the scope input data.

Driver mode (default):  

When the ResampleLocation is set to Driver, the resampling of the input time data is implemented in the 89600 VSA software - Infiniium scope "driver" digital decimating filter system block , see preceding VSA system block diagram. In "Driver" mode, the current measurement input data is not limited to 8.2 M pts of scope data. However, there are differences in some of the 89600 VSA operation and data results:

Driver mode VSA operating differences:

SampleMode

Sample Rate Actual

Sample Rate Actual displays a read only value of the actual oscilloscope sample rate in Sa/sec.

UserSampleRate

UserSampleRate selects the scope sample rate when SampleMode is set to UserRate. The actual sample rate selected will be the highest sample rate that is less than or equal to the user requested sample rate, up to and including the FullRate sample rate. By controlling the scope sample rate, you can directly influence the update rate of the VSA. This is because sample rate directly affects the number of points the scope must transfer to the VSA. Certain measurements can be made significantly faster by limiting the scope sample rate due to reduced data transfer requirements.

UserSampleRate can also be used to increase the maximum acquisition time available from the scope by specifying a lower sample rate. A lower sample causes fewer samples to be taken per second, which means a longer time record can fit in the capture memory of the scope.

For S-Series, V-Series, and X-Series oscilloscopes, the user is cautioned to use proper limits on span/center frequency/stop frequency according to the data sheet of the specific scope. The current API prevents the VSA from controlling the front end anti-alias filters; therefore, when anything other than full rate is in use, user is expected to limit the above parameters to allowed max values.

For example, with the S-series 8GHz scope, if user rate is set to 10GS/sec, the user is cautioned to stay within the corresponding valid BW of the scope at 4GHz. See the Keysight Infiniium Oscilloscopes topic for more information.

For X90000 Series oscilloscopes, the maximum sample rate is reduced when using paired oscilloscope channels. See the Keysight Infiniium Oscilloscopes with 89600B VSA Software (PN 5990-6819EN) Application Note for more information.

The following table specifies the possible sample rates when using the Infiniium Series Oscilloscopes with the 89600 Software.

Each scope model is listed next to its maximum sample rate. The scope can sample at that sample rate and all the sample rates below.

Sample Rates for Infiniium Oscilloscopes with the 89600 Software

Sample Rate

Infiniium Model Numbers

256 GSa/s

UXR0051AP, UXR0252AP, UXR0254AP, UXR0402A, UXR0402AP, UXR0404A, UXR0404AP, UXR0502A, UXR0504A, UXR0592A, UXR0592AP, UXR0594A, UXR0594AP, UXR0702A, UXR0702AP, UXR0704A, UXR0704AP, UXR0802A, UXR0804A, UXR1002A, UXR1004A, UXR1102A, UXR1104A

UXR0051BP, UXR0252BP, UXR0254BP, UXR0402B, UXR0402BP, UXR0404B, UXR0404BP, UXR0502B, UXR0504B, UXR0592B, UXR0592BP, UXR0594B, UXR0594BP, UXR0702B, UXR0702BP, UXR0704B, UXR0704BP, UXR0802B, UXR0804B, UXR1002B, UXR1004B, UXR1102B, UXR1104B

128 GSa/s

UXR0104A, UXR0134A, UXR0164A, UXR0204A, UXR0254A, UXR0334A

UXR0104B, UXR0134B, UXR0164B, UXR0204B, UXR0254B, UXR0334B

160 GSa/s

X95004Q7, X96204Q7, all Z-Series models ≥ 50GHz

80 GSa/s 6

X91304, X91604, X92004, X92504, X92804, X93204, X92004Q, X92504Q, X93304Q, all V-Series, all Z-Series models ≤ 33GHz

40 GSa/s 1

90804, 91204, 91304

20 GSa/s 2

90404, 90604, 9404, all S-Series models (2 channels)

16 GSa/s 2

all EXR models, all MXR models

10 GSa/s

90254, 9254, all S-Series models (4 channels)

5 GSa/s

9064

4 GSa/s 1,4

 

2.50 GSa/s 3

 

2.25 GSa/s 3

 

2 GSa/s5

 

1.25 GSa/s 3

 

1 GSa/s

 

500 MSa/s

 

400 MSa/s 3, 5

 

250 MSa/s

 

200 MSa/s

 

125 MSa/s

 

100 MSa/s

 

50 MSa/s

 

40 MSa/s

 

25 MSa/s

 

20 MSa/s

 

10 MSa/s

 

5 MSa/s

 

4 MSa/s

 

2.5 MSa/s

 

2 MSa/s

 

1 MSa/s

 

1 Not available when > 2 channels are active, except for Series 90000 scopes.

2 Not available for 9404 scope when > 2 channels are active.

3 Only available for Series 9000 scopes.

4 Not available for 9064 Scopes.

5 Not available for 9064 scopes when > 2 ch's are active.

6 Not available when oscilloscope channels 1 & 2 or 3 & 4 are active at the same time, except 90000Q Series and Z-Series scopes.

7 Only applies to RealEdge inputs.

UserSCPIPreset

UserSCPIPreset is useful for setting parameters on the Infiniium Series Oscilloscope that cannot be set directly from the 89600 user interface.

SCPI commands can be entered separated by semicolons. SCPI Query commands are not supported.

Verify that none of the commands conflict with the normal operation of the software.

The VSA software may not undo the effect of these commands when the parameter is changed or an application preset is done. For commands affected by a *RST, you can disconnect and then reconnect after removing the command or after doing an application preset in order to undo the effect of the command.

Whenever the 89600 VSA needs to preset the scope it will send these user SCPI commands followed by other commands from the VSA. Be aware that the VSA preset will overwrite conflicting user SCPI commands.

To enter SCPI preset commands, follow these steps:

  1. Make sure that the Infiniium oscilloscope is specified as the Logical Instrument in the Analyzer Configuration. Click Hardware > Configurations.
  2. On the Acquisition > Extended Settings tab, type in the SCPI commands separated by semicolons in the UserSCPIPreset parameter text box.

For detailed information on SCPI commands for the Infiniium Series scopes, refer to scope programming documentation.

For more information, see the Keysight Infiniium Oscilloscopes with 89600B VSA Software (PN 5990-6819EN) Application Note.